This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90C387A: R_FB state changes after boot-up

Part Number: DS90C387A

Hi,

I would like to configure DS90C387A to do "Rising Edge Data Strobe". However, the R_FB signal is driven to logic "0" during system boot-up. Then it will be driven to logic "1"  and stay as "1" as soon as the system boot-up is completed.

Would this cause problem for DS90C387A to do "Rising Edge Data Strobe" ?

Thanks!

  • Hello,
    When left open the R_FB input is low because of the internal pull-down. If the input is high the rising data strobe edge will be selected, so you should make sure it is set to high if you like to configure it to this.
  • Hi Palaniappan,

    I do not understand your response. This is not relevant to my question.

    The R_FB pin is always driven the entire time. My concerns is whether the R_FB pin status might be latched by DS90C387A during boot-up.

    Regards,

    John

    Palaniappan Manickam said:
    Hello,
    When left open the R_FB input is low because of the internal pull-down. If the input is high the rising data strobe edge will be selected, so you should make sure it is set to high if you like to configure it to this.

  • John,
    Sorry for the delayed response.
    This is an input pin, so there is no concern here regarding latching during boot-up. This should be ok.