This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90C387A: R_FB state changes after boot-up

Part Number: DS90C387A

Hi,

I would like to configure DS90C387A to do "Rising Edge Data Strobe". However, the R_FB signal is driven to logic "0" during system boot-up. Then it will be driven to logic "1"  and stay as "1" as soon as the system boot-up is completed.

Would this cause problem for DS90C387A to do "Rising Edge Data Strobe" ?

Thanks!