This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: DS90UB954-Q1

Part Number: DS90UB954-Q1

Dear Sir,

Pls advise to check about UB954 BCC_CONFIG(0x58) D[2:0] BC_FREQ_SELECT setting.

Referring to the description on spec, it should be configured to 50Mbps if our serializer is UB953.

But if we initial this register to 0x5e (BC_FREQ_SELECT -- 110 ; 50Mbps ) then we would get trouble to communicate via I2C.

Only setting to 0x5d (BC_FREQ_SELECT – 101 : 25Mbps), and the communicating  by i2c is working properly.

Do you know why i2c can’t be working properly if set BC frequency to 50Mbps.

Thanks, Ian.