Other Parts Discussed in Thread: DS90UB962-Q1
[ DS90UB964-Q1 ] Frequency Counter, RX_FREQ_HIGH & RX_FREQ_LOW
Hi,
My customer try to read and convert the readout value of RX_FREQ_HIGH & RX_FREQ_LOW to actual frequency value, however the calculated value does not match with actual frequency. See the table below.
Case 1
Register |
0x4F |
0x50 RX_FREQ_LOW |
Readout Value | 0x35 | 0x5C |
Calculated Frequency | 53 | 359375 |
53.359375MHz
Case 2
Register |
0x4F |
0x50 RX_FREQ_LOW |
Readout Value | 0x33 | 0x5b |
Calculated Frequency | 51 | 35546875 |
51.35546875MHz
For both cases, actual PCLK is higher than 90MHz, thus don't match.
Can you please let me know whether this conversion is valid?
Note: REFCLK is 23MHz.
Thanks,
Ken