Other Parts Discussed in Thread: HD3SS3212, TUSB320, TPS65982
Hello there,
I need, for my application, a USB Type C HUB, which connects to a USB 3.1 Type C available port on my host device and extends it to another USB 3.1 Type C port and a USB 3.0 output (doesn't need to be a port, as I might use it for another HUB later), and it seems to me that TUSB8044 is the right IC for this. But I'm not 100% sure it can solve my problems, as it seems, from its datasheet diagram, that it only outputs USB 2.0. Is this information correct?
Also, it looks to me that only this IC is not enough for doing this HUB, as can be seen from the "Application and Implementation" section on the Datasheet. Even though I don't need all of the resources the application offers, do I still need all of those extra circuits it uses for my application?
Thanks in advance,
Eduardo