Part Number: TUSB2046I
hi ti expert
now,my project is using tusb2046 which only support full speed as a bridge to connect a bgn wifi module , do the upsteam throughput test frome the wifi module, the result was so terrible that only 400bps,then unmount the hub instead fly line, the test speed was 28Mbps, wether of the hub's bottleneck that only up to 12Mbps not the high speed cause this difference? ths for your reply