Part Number: SN65DP159
Hello.
I am considering SN65DP159RSB.
I have a question.
Data sheet P9
Data Sheet 7.5 Power Supply In the Electrical Characteristics section there is a description of PD1, PD2.
The temperature of the Max value is Ta = 85 ° C.
Please tell me PD1 (MAX) and PD2 (MAX) at Ta = 40 ℃ and Ta = 50 ℃. (TEST CONDITION is the same as the condition of the date sheet)
Thank you.