This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDP158: TDP158, TDP158I Power consumption

Part Number: TDP158


Hello.

I am considering TDP158,TDP158I.

I have a question.

Datasheet P8
In the data sheet 6.5 Electrical Characteristics, Power Supply part, PD 1, PD 2 is stated.
The temperature of the Max value is Ta = 85 ° C.

Please tell me PD1 (MAX) and PD2 (MAX) at Ta = 40 ℃ and Ta = 50 ℃. (TEST CONDITION is the same as the condition of the date sheet)

Thank you.

  • Hello Ishii-san,

    We do not specify a max power consumption for max voltage / room temp conditions. We only specify a max power consumption for worst case conditions (max voltage, high temp).

    Regards,
    JMMN
  • Hello.

    Thank you for answering.

    We are currently examining system specifications.
    I am doing calculations on the power of the system.
    It is a state that we have to suppress electric power as a system.
    Therefore, I want to know the values at the temperatures Ta = 50 ° C and Ta = 40 ° C used this time.

    Please let me know if results can be obtained by simulation.

    Thank you.

  • We are not able to provide these results by simulation. From similar testing, we see that when running at nominal voltages at 40/50C, power consumption is close to the typical range.

    Regards,
    JMMN