Part Number: TCA9546A
Other Parts Discussed in Thread: PCA9546A
Hi team,
I'm an FAE supporting some industrial companies in Japan.
My customer provided some questions.
Datasheet shows Vpass=1.6V~2.8V@VCC=3~3.6V.
It means 1.6V~1.8V is acceptable for pull-up voltage @VCC=3~3.3V.
Is this understanding correct?
Or does it mean output voltage will vary from 1.6~2.8V?
While, the customer considers following configuration.
- 3.3V input(master) from MCU
- I2C IC will be operated at 1.8V.
If you have any advice regarding connection, pull-up etc please share them.
Best regards,
Shota Mago