When we plug in a thumb drive into the TPS65986 type C port, we can see it and read the thumb drive.
If we unplug it and then re-insert it, we cannot see it. If we reboot, we can now see it again.
We have GPIO0 set to detect if something is plugged in, it’s a 1 if something is plugged in and 0 if not.
GPIO1 is set to indicate if we are a Host 0 or Device 1 and that works.
You have the schematic and TPS65986 configuration. Any idea what might be causing this? Are changes to the configuration required?