Part Number: TCA9617B
There is only Ta 85 degree in datasheet. what's Tj of TCA9617B?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Ryan,
Typically the calculation you made is correct however this device does not dissipate very much power.
Let me expand on this a bit. The 30mA of current will flow through our pull down FETs which will dissipate heat. Now calculating the power dissipation follows:
Rdson(max) = VoL(max)/IoL(max)
0.23V/0.030A=7.67 ohms
Power = R*I^2
Therefore power across one FET is as follows:
P=7.67 ohms * (0.030A)^2
6.9mW
We have two FETs which can pull low therefore: multiply the power by 2 = 13.8mW
Now calculating Tj using theta JB as it seems you have used this value of 90C/W:
Tj=85C+0.0138*90
"How can Tj 85 degree match Ta 85 degree?"
Tj = 86.242 which is ~85C
Sorry if my original answer seemed confusing. I answered based on my assumption this device would not dissipate much power at all.
"Does below statement from Logic team also fit your device?"
I actually do not see the full link you are referring to. If you are looking for absolute max junction temperature then I would think it should match the storage temperature max but this isn't always the case. If the customer is asking for an absolute max junction temperature then I would suggest 125C is the number you provide.
Thanks,
-Bobby