Part Number: UCC21520
Hil,
I am using driver UCC21520ADW for driving the GAN FET from my PWM controller.
PWM controller
Vgate high:10.5V
Vgate low:1.5V(max) at Isink=5mA
UCC21520ADW:
Vih:1.6V(min)
Vil:0.8V(min)
PWM controller switching frequency:1 MHz
What would be the sinking current flows to the PWM controller?
UCC21520ADW also has an internal pull down of 200k ohm.Is it sufficient to sink the current?
Thanks in advance,
Selvam.