Part Number: TIOL1115EVM
Other Parts Discussed in Thread: TIOL1115
I am using the TIOL 1115 EVM along with a IO Link Master from TEConcept.
I have an M12 cable connected to the Master and I cut the other end and stripped the wires to connect the L+, C/Q, and L- lines to the EVM in the TB2 socket (AMP connector where you put in wires and screw in to tighten them in place).
I've noticed that the L+ line is gets noise on every rising edge and falling edges of the C/Q line by almost 100 mV. I am using the LDO to supply 5V to an MCU, so I can't have this much inconsistency. I've tried to research on what the problem could be, and it seems like the wires may be experiencing electromagnetic interference because they are not shielded?
The way TIOL 1115 EVM is designed, if I want to input all three lines (L+, C/Q, L-), I need to connect the wires to TB2 socket, and I don't know if it's possible to have them "shielded" so the L+ line does not get bothered by the C/Q line. Does anyone have any ideas on how to fix this? Did anyone else have this issue?