Part Number: TPS65987D
I am working on a device which will only work as power sink (UFP) and I am not sure what I should do with the PP_CABLE connection. I don't think it is used in a sink application.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65987D
I am working on a device which will only work as power sink (UFP) and I am not sure what I should do with the PP_CABLE connection. I don't think it is used in a sink application.
Thanks
Hi Daniel,
Ideally, you can ground the PP_CABLE pin for the sink only application. However, I would suggest you to connect it to 5V rail so that the option is available to source VCONN if the design requirement changes in future.
If this answers your question, PLEASE select This resolved my issue.
Thanks,
Rahul