Hi,
DS90UB933-Q1 for tis part. I read from the datasheet.
1. I using External oscillator mode,
If My external crystal is 50 MHZ for 12 Bit Mode , PCLK input to TI's 933 have to be 100Mhz based on Page 20 of your datasheet. Can I use lower value other than 100Mhz fr PCLK input to TI's 933?.
Cos My Image sensor output can only support output up to 74Mhz Max. Or I need to change my External clock to achieve this?
2. Alternatively if I use 48 Mhz for 12 Bit Mode , My PCLK input to TI's 933 have to be 72 Mhz. . For this case I cant use for 10 bit mode if my image sensor can only support up to 74Mhz.. I have to lower down my external Crystal MHz .
Thank You very Much