Part Number: PCA9306
Hello,
Is there a malfunction situation when power up or power down when we configure figure 7 of the datasheet?
VREF2 pin capacitor charge and discharge are delayed due to time constant of 200kohm and capacitor value.
When power cycle which very short VREF2 OFF time duration happens, VREF2 capacitor may still have voltage due to this time constant.
In this case, VREF1 side condition doesn't define but is there a condition which PCA9306 falls malfunction condition?
There were devices to define power cycle requirement for POR. For example, next power up should be done after power supply voltage becomes less than 0.5V for example. I would like to confirm if PCA9306 doesn't fall unstable state when power cycle is applied medium power supply voltage.
Best regards,
Toshihiro Watanabe