Part Number: AM26LV32E
Hello,
My customer has a question about AM26LV32E.
[Q]
VID = VA - VB ?
According to D/S p4 6.1 Absolute Maximum Ratings (4), Differential input voltage is measured at the non-inverting input with respect to the corresponding inverting input.
A = non-inverting
B = inverting
So, I think VID = VA - VB.
When VID = VA - VB > 200mV, Output = H.
But accordimg to D/S p7 Figure2, Outpput = H when VA - VB = -1V.
Is my understanding wrong?
Best Regards,
Kaede Kudo