Part Number: DS90LV004
Hi Team,
I'm looking for a device that can drive a high number of LVDS lanes (up to 14 lanes), each with a signaling rate of 800Mbps. The goal is to transmit this data from one board to another through a 10m cable. So, this leads me to 2 different questions:
Question 1.
What would be the best part to suggest as well as typical configuration? The DS90LV004 looks to be a good fit, but I would like confirmation on if this can drive to 10m? Would I need one DS90 on the TX board and another DS90 on the RX board?
Question 2.
Do you have any recommendations for standard off-the-shelf cables that can support these requirements? Ideally, I'm looking for a cable that has a high density of lanes.
Thanks,
Mitchell