Part Number: DS110DF111
We have two retimers on out latest design that we cannot seem to get configured using the eeprom.
To start with how does the DS110DF111 know the physical address of the EEPROM?
If I use a 24C02 EEPROM, its A0, A1, A2 pin can be configured to create an SMBUS (write) address between 0xA0 thru 0xAE.
Does the DS110DF111 expect a certain address that must be used? If so what is this address?
Can you provide me with a simple hex file that will work with two devices that are chained? Just so we can test both devices?
The physical address of our re-timers are 0x34 and 0x36.
Will the device keep reading bytes from the eeprom until address 0xFF ? or will it stop prior to that