Part Number: TUSB8041
How do I get a hold of the Windows software to configure the TUSB8041 USB hub?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB8041
How do I get a hold of the Windows software to configure the TUSB8041 USB hub?
Hello Sarah!
Just looking to clarify, do you mean the software to configure an EEPROM with the TUSB8041? If so, here is the zip file with the programmer and the user guide!
If you mean to write to the registers via SMBUS mode, you must write to it with an SMBUS capable host controller. For more information on the configurable modes, please see section 8.4 in the datasheet.
Please let me know if this answers your question.
0636.Texas Instruments TUSB8040 EEPROM Programming Utility (Version 1.0).pdf
7230.TUSB80xx_EEPROM_Programmer_V1.0.0.1.zip
Best,
Gerasimos
Hi Gerasimos, our board uses the TUSB8041, which provides our card with both a standard USB and high speed USB connection. The name, for instance, shows up as:
"Generic SuperSpeed USB Hub" and "Generic USB Hub"
We would like to rename this nomenclature to something of our own choosing, so for instance:
"Smurfs Rock SuperSpeed USB Hub"
"Smurfs Rock USB Hub"
I was told by our electrical engineer that there is a Windows tool, which allows us to set the name. Which of the above would do that or something else? Thanks in advance,