Part Number: SN75DPHY440SS
Hi,
I am trying to link up 2-3 MIPI extender cables together. I am using flexi-cables to link up the extenders and the cable length is approx. 30cm. I am having issues trying to get an image from the sensors to the processor ISP. It works fine when using one MIPI extender cable but more than one extender cables, it doesn't work. The I2C clock to the sensor is 100khz and the signals looks good on the scope. The processor clock 8mhz is fed through the cable to the sensor.
Regards
Paul