Other Parts Discussed in Thread: SN75DP130, SN65DP141
product Broadcast camera ,viewfinder HDMI/DisplayPort interface alternate mode USB-C
We have changed our viewfinder standard from HDMI to DisplayPort.
My question is:
1-can we still use the sn65dp159 rsb (40 pin package) for DisplayPort retimer. I was reading apn slla358 “dp159 ad dp retimre and the write about the 48 pin rgz package?
2- in another design I noticed that a sn75dp130 retimer is used? What do you suggest?
Right now I have the following:
Source:
Xilinx DP core>dp159>tusb1046 switch>cypress ccg3 PD ctrl>USB-C
Sink:
Viewfinder:
USB-C>cypress ccg3 PD ctrl> Altera DP core (no switch , no retimer)
I am a bit worried about the AUX signals and how the dp159 and the tusb1046 will work. For power reasons we want to switch from 4<=> 2 DP lanes.
Thanks in advance
Ron