Part Number: TPS65982
Hi,
Is there any way download application code to TPS65982 via SWD interface? after then it should be possible to write flash via I2C with 4CC commands ..
Umit ..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65982
Hi,
Is there any way download application code to TPS65982 via SWD interface? after then it should be possible to write flash via I2C with 4CC commands ..
Umit ..
Hi Umit,
The SWD lines are only used internally for our FW team debug. We do not recommend the customer using the SWD interface. The first time you bring up a board with the TPS65982, you should use the SPI interface and program the SPI Flash. Afterwards, you can update the TPS65982 over I2C by following the steps in this app note: 
If this answers your question, PLEASE select This resolved my issue
Thank you,
Eric