Part Number: DS125BR800A
How can the DS125BR800A not enable PCIE, SAS/SATA protocols, only need to output the input differential signal, and can set EQ value?
The current operation is through the I2C configuration register
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS125BR800A
How can the DS125BR800A not enable PCIE, SAS/SATA protocols, only need to output the input differential signal, and can set EQ value?
The current operation is through the I2C configuration register
Hi,
The DS125BR800A does not track PCIe or SATA/SAS protocol. It can be used with any AC coupled differential signal.
There are a couple key registers to control
Register 0x06 = 10'h (default). Change to 18'h to enable SMBus interface control.
The equalization settings may not be ideal for your application. I recommend to start with a low setting and increase the value slowly.
For example:
CH0:
EQ Register 0x0F = 00'h
DEM Register 0x11 = 00'h
Regards,
Lee
Hi,
I would recommend to force the signal detect function "on". It is possible the amplitude is not enough the keep the device active.
Write registers: 0x0D = 02'h, 0x14 = 02'h, 0x1B = 02'h
Can you send a picture of the input and output waveforms?
What is the datarate?
Thanks,
Lee
hi Lee,
When set 0x08=0x58, the output signal can be adjusted by EQ register, and when increasing form 0x00 to 0x09 it works.
But the output does not enlarge the amplitude when increasing value form 0x09 to 0x0f , and it seems that the EQ is not linear while the register 0x04 = 0x00.
The datarate is between 0.5G ~1.6G. It varies according to different settings.
Any suggestions?
Setting 0x08 = 58 does three things:
1. Overrides the signal detect pin functionality
2. Sets Idle control to the registers
3. Overrides RXDET
For a low datarate and low amplitude signal I would just force the signal detect "on" as I described in my previous post.
At these lower datarates you are not going to get a large gain from the equalizer, it is tuned to provide maximum gain for 10 Gbps signals.
The equalizer is linear to a point, and the output driver will also impact the total device response. Since you are "floating" the MODE pin, the output will be in limiting mode for these low datarates. The voltage gain you see is coming from the driver circuitry after the CTLE function.
Regards,
Lee