This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DPHY440SS: Connecting multiple SN75DPHY440SS based MIPI cables in series?

Part Number: SN75DPHY440SS

Hi 

We have created a DPHY MIPI CSI FPC extension cable based on the SN75DPHY440SSRHR design:

The track length between the Connector to the Camera and SN75DHY440 retimer is ~200 mm

The track length between the Connector to the Processor and SN75DHY440 retimer is ~35 mm (see below)

From Camera  ------------200 mm ---------------------   SN75DPHY440 Re-timer -------------------------- 35 mm-------------------------------  To Processor

 

We have tested images with 1280x800 (resolution) with 120 fps frame rate with only 2-lane MIPI connected, with just a single MIPI Extension cable everything works.

But as we trying to connect 2x MIPI extension cable in series together, the processor started to lose sync with the frame and in some cases not able to pick up any frame at all.

As I do not have a decent scope to measure the MIPI bus, making debugging rather difficult, wondering if someone else have tried similar design and could shed some light?

Thanks


Thomas