Part Number: SN65HVD52
The SN65HVD52 is "fully enabled with no external enabling pins. I'm used to 485 chips with a DE/RE pins."
If the Tx line is always enabled, how will this work in 485 multidrop connections. Would this the SN65HVD52 only work as a master? Or can this chip be used with multiple slave devices? If not, would I have to use the D53/54/55 series with DE/RE pins?
Thanks.