Part Number: LMH1297
Hello,
The model of LMH1297 is being analyzed in ADS.
There are
ReTimer configuration, Cable Input, Cable Output
and
ReTimer configuration, FR4 input, FR4 output
samples in the LMH1297 model, but there is no "Cable Input, FR4 output" sample.
I created a file E that combines C and D and analyzed it, but EYE does not open.
Is there a sample file that EYE opens at RX part with the following configuration?
TX (Tx_cable_75m.ibs) → Cable(75m) → BNC → Line (75 ohm) → LMH 1297 → Line (100 ohm) → RX
Best Regards,
Tetsuya