This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2560: Maximum of 0,66V Vil

Part Number: TPS2560
Other Parts Discussed in Thread: TPS25221, TPS2062C, TPS2065C

Hello,
i would like to use the low active TPS2560 as USB3.0 Powerswitch.

My Problem ist that the TPS2560 has an Maximum low Signal of 0,66V. My USB3.0-Host Controller is the VIA VL805 which has an Maximum Vil of 0,8V. (Vih 2V).

Is there any Texas Component wich preferes higher Signals as low Signal ??


regards