Part Number: TPD4E05U06
Hi,
I'm planning to use TPD4E05U06DQAR for an HDMI 2.0 design. In the datasheet pin numbers 6, 7, 9, and 10 are listed as NC on the package pinout. However, in the Applications section 8.2.1 Figure 14 shows pins 6, 7, 8, and 9 as D1-, D1+, D2-, and D2+. Should I connect these NC pins to the respective data pins? I see the recommended layout has the signal running under the NC pins so it would make sense for them to be connected, unless the layout example has them on a different layer than the part.
Thanks,
Briana