Part Number: TCA9800
Other Parts Discussed in Thread: TCA9517, , TCA9509
Hello team,
It may be a fundamental question, but could you instruct me about VOL on the B side difference TCA9800 vs TCA9517?
I found the following sentence on the application report(SLVA878: www.ti.com/.../slva878.pdf) and wonder what is the key point from the device internal structure point of view or I2C application specific reason.
"This VOL and VIL mis-match is common, especially when a buffer device with a voltage offset is used. Most
of these common buffers will have a fixed VOL output of 0.5 V. The TCA980x helps with these issues by
providing a very low VOL signal on both the A and B sides. The A-side typical value is below 0.1 V and the
B side typical VOL is 0.2 V"
My questions are;
1) Why most of the buffers(such as TCA9517) have VOL output offset of 0.5V?
2) Why the VOL offset is generated only on the B side?
3) What is the main reason why TCA9800 can sustain lower VOL?
Thanks in advance.
Shinya Sawamoto