This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822H: About Reset Timing

Part Number: DP83822H

Hi Team,

Figure 2. For Reset Timing, T2 is specified as 2ms (max).

At Rev. A (SNLS 505 A), it was 195 ms typ.Is Max 2. ms of Rev. C correct?

Another, T1's NOTES "X1 clock must be stable for a minimum of 1 μs during RESET pulse low time"

Does this means that XI needs to stabilize within 1 μs after the RESET pulse changes to L?

Best Regards,

Kenji

  • Hi Kenji,

    The updated version is correct.
    What the clock stabilization time is saying is that for RESET to occur properly the reference clock needs to be stable for at least 1uS during while RESET is LOW.
  • Hi Ross,

    Thank you for answering.
    Is there a minimum for Reset Timing's T2? How many should Typ value be targeted?
    Although Power - Up Timing is specified as T2 = 200 ms (max), is it also necessary to wait for a RESET pulse to be applied after the power is turned on?

    Another thing, there is no MDIO waveform in Figure 2.
    What kind of waveform is correct for MDIO?
    Is there a waveform?

    Best Regards,
    Kenji
  • Hi Kenji,

    There is no minimum. You should not try and access MDIO/MDC until the 2ms expires. That is the reason why there is no typ or min value listed.
    For POR, there is no need for you to apply a RESET. This is done internally by the PHY. All you need to do is wait 200ms before accessing MDIO/MDC.

    MDC is just a clock waveform at whatever frequency you are operating it at.
    MDIO is just a toggling CMOS line with whatever pattern you are transmitting or receiving.
    This bus timing image here is a good example: en.wikipedia.org/.../Output