Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
The pin numbers shown in Figure 42 in the datasheet for the TPS65987D do not match the Pin Description Table or the TPS65987 - 90EVM board schematic. Can you correct Figure 42?
There are many differences, but here are a few.
| Pin | DataSheet Description | Figure 42 |
| 11 | PP_HV1 | VBUS_1 |
| 12 | PP_HV1 | VBUS_1 |
| 8 | Drain1 | ADCIN2 |
| 7 | Drain2 | LDO_3V3 |
| 9 | LDO_3V3 | PP_HV1 |
| 10 | ADCIN2 | PP_HV1 |
| 13 | VBUS1 | GPIO0 |
| 14 | VBUS1 | GPIO1 |
| 15 | Drain1 | GPIO2 |
| 16 | GPIO0 | GPIO5 |