A customer has an application that uses a RTOS called On-Time. It’s similar to VxWorks. They have a TSB81BA3A chip. They have a low level driver that was written specifically for this chip to work for the On-Time RTOS.
Their application is running at S400b and this has worked for the last 14 years J
They have a NEW project which requires us to run at S200b. They thought they could just change the speed and of course they now found out we can’t with this chip.
Their question is how portable do you think their driver code will be if they replaced our current Fire wire card to one with the TSB41BA3x chip so we can run at S200b. How similar are the cards? Do you think a complete overhaul of the driver code will be needed OR do you think the chips are similar enough it should be a straight forward port?
Would love to hear your feedback.