Part Number: DS90UB947-Q1
Hello Sirs,
Can ds90ub947 this chip work if mode_sel[1:0] pin and ID pin setting properly ? Don't need i2c register setting,right ?
power up sequence follow 1.8V -> 1.1V -> PDB -> open LDI input
power up ramp fast than 1.5ms
Another question is will ds90ub948 have default screen output when 947 link with 948 but no open LDI input to 947 ?
Many thanks !