Part Number: TPS65987D
Other Parts Discussed in Thread: BQ25713,
Can the reverse boost feature of the bq25713 charger (5V) to be used as the source for VCONN (PP_CABLE) as well as the peripheral source path through VBUS (PP_HV2) for the TPS65987D?
This would eliminate having a separate 5V system source for the PP_CABLE pin by using the 5V source from the reverse boost on the charger.
These questions relates to timing, as the requirement is to source up to 600mA which could be sourced from the bq25713 charger if the VCONN timing is sufficient.