Part Number: TLK10232
We need two ports converted from 10GBase-KX4 to 10GBase-KR. I am looking at the TLK10232 part which looks promising, though it calls out XAUI-to-KR only. I saw one mention in a support forum that indicated that this part would not function with 10GBase-KX4 instead of XAUI, though it was unclear why - due to specific configuration in one application instance or a wider limitation of the part itself. Later, I saw some reference to making it work provided that the SERDES was configured to work for KX4.
So - what specifically would limit this part from functioning with a 10GBase-KX4 interface rather than XAUI?
- James