Part Number: SN65HVD233
I need a CAN extender chip on an interface board that takes CAN_H and CAN_L signals from CAN BUS A and makes a separate CAN BUS B. I have legacy designs that did this with the AMIS-42700. The AMIS-42700 needs 5V and I don't have easy access to 5V in a new design. I have 3.3V. Creating the 5V on the interface board is difficult for some reasons that I won't go in to. Since I only have 3.3V volts I'm trying to come up with a way to make an extender from two SN65HVD233 chips (or something similar). Would it work to hook two SN65HVD233 the way I have shown below on my interface board?