Part Number: TPS65987D
Other Parts Discussed in Thread: TUSB322I
Hello,
I am looking for assistance selecting the correct USB Power Delivery chip for our application. First, let me start off by saying I am a mechanical engineer and therefore my understanding of the USB spec is limited and some of the terminology goes a bit over my head.
I am trying to design a cable to go from a mobile device (EUD) to a tactical hub. The EUD in this case is a Galaxy S8 but that shouldn't matter as I want to design the cable such that it is compatible with most if not all USB Type-C ready devices. The tactical hubs are capable of communicating via the 2.0 standard as well as the 3.0 standard and can supply 5V power at 2.5amps. It should also be noted these tactical hubs are not yet 3.2 compliant and therefore provide no means to communicate via the CC pin or provide any power regulation at the higher PD voltages.
The idea for the cable is that we have an inline PCBA with the PD chip on it which allows the EUD to go into sinking host mode or more appropriately said we want the EUD to be the data source and the power sink. Previously our end users would accomplish this with either a custom ROM on the EUD or a specific resistor value between ID and GND (assuming the device had built in support for that mode) or a combination of both. With the new PD protocol we can achieve this without the custom ROM, which is very attractive to our customers.
Since I am an ME and work for a mechanical design firm we have partnered with a firm to help develop the PCBA. Unfortunately they are not well versed in the latest USB specification and as a result we are struggling a bit to move the design forward (ideally we partner with someone else but that isn't an option). In an effort help I am reaching out to this community to see if I can gather the information needed and educate myself well enough to move development along. There is one other high level goal beyond what was stated above and that is we would like the design to allow for the future integration of a USB hub circuit so that we may integrate other capabilities such as analog audio, or an Ethernet to USB adapting, or simply connecting another USB peripheral. It's not absolutely critical that this additional feature makes use of the same PD chip. In fact this secondary requirement may be the source of our issues...
Finally, the partner firm's initial thought was to move forward with the chip identified above, TPS65987D. We have managed to work through most of the issues but there is one final sticking point. They have indicated there is an issue with power regulation and from what I understand it has to do with how the PD spec defines the need to be able to handle 5V, 9V, 12V, and 20V and therefore needing a buck/boost circuit. I understand what buck and boost circuits do but if I have a constant 5V source I am not sure why we need to concern ourselves with these higher voltage capabilities. Could it be that this isn't the correct chip for our application? Any help here would be much appreciated.
Thanks in advance,
Mike