This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983: TPS65983 Authentication test problem

Part Number: TPS65983

Hi all:

What is the tps65983 value of the current limiter

The customer did a short circuit test at 5 V 3 A,9v 3A and there was no problem。

A problem arose when the customer did a short circuit test at 15 V3 AAfter power off ,TPS65983 can not work

What causes it,and How to improve this problem