Part Number: DS90CR286A
Other Parts Discussed in Thread: DM385, DM388
Hi,
I have a IC to interface camera link signals to get LVCOMS o/p
Camera link LVDS differential pair signals -->---DS90CR286A-->--- 28 bit LVCMOS o/p-->--- DM385 Video Input
Similarly can I use the same IC for BTU656 LVDS video input signals instead of camera link?
Please suggest an IC to interface BT.656 LVDS signals
BT.656 LVDS signals (There are no positive and negative signals)--->--- IC??--->--- 28 bit LVCMOS o/p--->--- DM385 Video Input
Or can the DM385 directly take BT.656 video inputs, if yes please specify the pin numbers which can take BT.656 Video inputs in DM385/DM388
Kindly answer my questions appropriately.
Thanks & Regards
Krishna