Part Number: TUSB8020B
Other Parts Discussed in Thread: TUSB9261
Hi. I have this Ic on a PCB. Device driver sees the hub, but leaves it as "Unknown Device". I have an un-programmed I2C EEPROM connected. Per the datasheet, the Hub goes into "programming mode". However I can't find any definition in the datasheet explaining how to program the device in programming mode. (The words "programming mode" are only used once in the datasheet.)
I looked in the eval kit datasheet, and under trouble shooting there is a note "Make sure that the latest drivers are installed for the host controller." Where can I find these drivers?
For the EEPROM, the following is noted in the Eval kit datasheet:
"The EEPROM interface defaults to programmable (not write-protected) so that any installed EEPROM’s contents may be modified to test various settings. If an EEPROM data change is required, the values may be changed using the register access methods outlined in the TUSB8020B data sheet. In addition, a Microsoft® Windows® based EEPROM utility is available upon request."
Can I get the EEPROM utility?
I'm going to try disconnecting the I2C IC to see if that helps. However I would like to be able to program this IC on the PCB going forward (my qty is too low for pre-programming).
Thanks
Tim Anderson