Part Number: DP83620
Other Parts Discussed in Thread: TS3L501E
Hello,
I need support in the Hardware design part of DP83620.
This IC provides a common output TX+/- and RX+/- for both Copper and Fibre mode and there are some strapping options to configure the IC in either modes.
My application requires both these modes to be designed on the PCB and should be field configurable. Now based on the evaluation kit it contains a set of 0 ohms resistor which can be stuffed or removed to use either of Copper or fiber mode however this cannot be done in the fields once the product is designed.
One way is using a Jumper or switch to achieve this where I am skeptical about the performance since this is a high speed part they signals are bound to get disturbed with these solution.
Kindly provide a suitable support.