Part Number: DP83867CR
When debugging the auto-negotiation function of DP83867 , if the device is connected to the H3C 100M exchanger, it can be automatically negotiated to 100M. If the device is directly connected to the PC network port by using the 100M straight-through cable, the computer network port (supporting Gigabit/100M/Ten megabytes) is configured for auto-negotiation and the status of the computer network port is 100M. But the device still displays 1000M. Why is it not auto-negotiated to 100M?