Other Parts Discussed in Thread: DS90UB948-Q1
Hi, all
In my designed, the DS90UB921-Q1 support to RGB888, so that GPIO[0:3] can be used to GPI for input signal. and the GPO_REG[4:7] are output. how can I pass the input signal from DS90UB921-Q1 ?
May I use the blew ideas ?
1. Use the I2S_DA and I2S_WC to pass the input signal ?
2. Use I2C of the DS90UB948-Q1 to set GPIO[0:3] of DS90UB948-Q1, so that I2C control GPIO[0:3] of DS90UB948-Q1 output ?