Part Number: TUSB8044
Hello there,
I'm trying to use the TUSB8044 with a TPS65987D as the PD Controller, but I'm having some issues figuring out the Billboard related pin's connections. On the TUSB8044 datasheet, it mentions that the PD controller has to configure the Billboard function in the TUSB8044 and store Billboard information on an external EEPROM, as follows :
I don't understand exactly how to connect these BBbmConfigure pins on my PD Controller. If I want to use TUSB8044’s default values of the Billboard Capability Descriptor, without the EEPROM, do I still need these pins to be connected?
Thanks,
Eduardo