Part Number: DS90UB954-Q1
Do UB954 have a function to transmit different data from TX Port0 (CLK0,D0,D1) and TX Port1 (CLK1, D2,D3) ?
I want to realize the following operations simultaneously.
1.The Data-A received by UB954.RX Port0 is transmitted to UB954.TX Port0 (CLK0,D0,D1).
2.The Data-B received by UB954.RX Port1 is transmitted to UB954.TX Port1 (CLK1,D2,D3) .