Part Number: SN65LVDS101
I am using the sllc125a.ibs model for simulating the SN65LVDS101, and am seeing unexpected behavior in the signals. The positive and negative signals both seem to have skewed duty cycles, so that high pulses are very wide and low pulses are very narrow as seen in the attached image. I am expecting to see a normal, balanced LVPECL signal here and can't find anything on my end that is causing the skew.
My simulation is being done in Hyperlynx LineSim @100MHz.
The issues I'm seeing with the signals are:
- Expecting 800mV swing, only seeing ~600mV
- Duty cycle issue
Looking for any assistance in getting this model properly set up, or reasoning behind this behavior.