Dears:
There are 3 questions about DS90UB960 of supporting sensor modules as follows:
1. I know 960 can connect 4 sensor modules, if 960 is connected only 1 or 2 or 3 sensor modules, how can we design it? Or ignore the unused channels?
2.I know 960 can support 2-Megapixel Sensors with Full HD 1080p Pesolution at 60-Hz Frame Rat.
If the sensor is less 2-Megapixel or 30Hz Frame Rat, can 960 support the sensor? Or is there any parameters set?
3.Can 960 support 4-Megapixel at 30-Hz Frame Rat?
Pls. give some advice.