This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: There are 3 questions about DS90UB960 of supporting sensor modules.

Part Number: DS90UB960-Q1


Dears:

There are 3 questions about DS90UB960 of supporting sensor modules as follows:

1. I know 960 can connect 4 sensor modules, if 960 is connected only 1 or 2 or 3 sensor modules, how can we design it? Or ignore the unused channels?

2.I know 960 can support 2-Megapixel Sensors with Full HD 1080p Pesolution at 60-Hz Frame Rat.

   If the sensor is less 2-Megapixel or 30Hz Frame Rat, can 960 support the sensor? Or is there any parameters set?

3.Can 960 support 4-Megapixel at 30-Hz Frame Rat?

Pls. give some advice.

  • 1. I don't know whether I understand your key point. For hardware design, please refer to d/s page4 on RINx+/0 description. For software setting, it is dependent on your selected channel setting.

    2. Yes, it can support.

    3. Yes, please secure the data rate is following within the CSI2 bandwidth (~3Gbps for sync. mode with continuous CSI2 clock), which is listed in d/s.

    regards,

    Steven