Other Parts Discussed in Thread: BQ24232H
Hi
I have a portable device with a Li-on battery that gets charged via a constant current of 100mA from the USB port and an inbuilt charging IC.
However i have a concern regarding the kind of power source/USB port it could possibly be connected to. A USB 2/3 without enumeration or high power charger could kill the device.
What i am looking for is a part that can help identify if i'm connected to a 100mA source (USB 2 for ex.) so i can directly use this to charge OR if the device is connected to a high power source (USB 3/wall /fast charger) then to switch it through a current limiting circuit.
Any help is appreciated.
Thanks and regards